Part Number: RM57L843
Tool/software:
Hi, I am compiling a sample code for RM57L843 using two compilers: TI ARM Compiler 16.9.4 (CCS) and the GNU Arm Embedded Toolchain. The code execution time when using TI compiler is less when compared to GCC. I have kept optimization OFF in both the builds and matched all the flags including the use of HW floating point. The only difference is the default --opt_for_speed=1 used by the TI compiler. What could be the equivalent flag to this, to be used in GCC so that both have almost similar execution time?