Part Number: MSPM0G1505
Other Parts Discussed in Thread: MSPM0G3507
Tool/software:
Hi,
We are looking to use the 2 x GPAMP in MSPM0G1505 to measure differential voltage from an ASIC. The ASIC has VSENSE+, VSENSE- signals which provides the actual voltage at the Die on the Core and GND rails.
The proposal is to use the 12 bit A/D of MSPM0G1505 with the Two OPA's in Difference Amplifier Configuration to measure the voltage at the Die (Fig 12-8 in Slau846a.pdf).
The MSPM0G1505 with the GPAMP will be replacing ADS1015IDGST, Is it possible to comment on the suitability of this configuration for our use case. Also - is there a sample project available which we could use to test the implementation?
thanks