Part Number: AM2434
Tool/software:
Just want to check my understanding.
The AM243x PRG0 PRU1 - if set for EGPI 28-bit Shift-In, the PRG0_PRU1_GPI0 pad is used for the DATAIN.
On the TRM, the remaining GPI1~GPI19 pads are greyed-out (Table 6-412. PRU GPI Signals and Configurations)
Does this mode force the remaining GPI1~GPI19 pads into EGPI mode, so they can't be MUX'd for other functions?
Or is it possible to set the pad that would have been GPI15 or GPI19 for ECAP operation?
According to the Datasheet, PRG0_ECAP0_IN_APWM_OUT is mapped to F3 or M4, which are also the GPI15/GPI19 pads.