Part Number: MSPM0L1304
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
In the data sheet I can find 4 pins in “Table 6-3. Signal Descriptions” which can be woken up from ShutDown mode: PA0, PA1, PA17, PA18
According to “Table 6-1. Pin Attributes”, the controller “MSPM0L1304” only has two wake-up pins.
CCS also only suggests the two pins “PA17” and “PA18” for the wake-up function.
Is the data sheet wrong at this point or can the pins “PA0” and “PA1” also be woken up from ShutDown mode?
If this is possible, how do I implement this in CCS?
Best regards,
Christian