This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, TI expert.
I made AM2634 test board and put the "WARMRSTn" pin floating.
When I powered my AM2634 test board, I watched only low signal on "WARMRSTn" pin.
When I added 10k-Ohm pull-up resistor, I found high signal with 3 ms delay after PORz signal.
1. In AM2634 datasheet, the pin type of "WARMRSTn" is "IO".
Is the method using pull-up resistor right?
2. It seems that I can set internal pull-up resistor for "WARMRSTn" via "MSS_IOMUX_WARMRSTN_CFG_REG".
But I can not find APIs dealing the registers.
I found "soc_rcm.h" and "soc_rcm.c" but they does not control "MSS_IOMUX_WARMRSTN_CFG_REG".
Hi Jeeuk Chang,
In AM2634 datasheet, the pin type of "WARMRSTn" is "IO".
Is the method using pull-up resistor right?
As mentioned in the datasheet, Warm Reset pin can be both Warm Reset Request (Input) and Warm Reset Status (Output). The Warm Reset Status output is pulled high after POR is de-asserted and a certain delay, as shown in the below picture from datasheet and hence a pull-up resistor is not required.
It seems that I can set internal pull-up resistor for "WARMRSTn" via "MSS_IOMUX_WARMRSTN_CFG_REG".
But I can not find APIs dealing the registers.
I found "soc_rcm.h" and "soc_rcm.c" but they does not control "MSS_IOMUX_WARMRSTN_CFG_REG".
You can configure that using the file \source\drivers\pinmux\am263x\pinmux.c
Hi, TI expert.
I could change IOMUX settings of WARMRSTN pin using "pinmux.c"
But, without external pull-up resistor on "WARMRSTn" pin, its output is always zeros.
With external pull-up resistor on "WARMRSTn" pin, its output is high after PORz with a delay.
-
This table is my result.
I changed the values of IOMUX_WARMSTN_CFG_REG at CCS.
The output pin of WARMRSTn is connected to TPS22918 load switch input.
-
From my result, I concluded ...
1. WARMRSTn is open drain output.
2. Internal pull-up resistor for WARMRSTn does not operate.
3. Internal pull-down resistor for WARMRSTn is 20 kΩ and can be used.
4. Output override "0" for WARMRSTn can be used.
Hello,
Apologies, I missed that WARMRSTn is Open Drain pin. You're right, we would need an external Pull-up of 10kohm as present in the EVM schematics.
Hope your query is solved.
Regards,
Sahana