Tool/software:
Hi,
I have two questions about flash bank memory size in MSPM0L-1228.
As show in the image below, the size of Code (Flash Bank 0/1) memory region is from 0x0000.0000 to 0x0001.FFF8 ( or 0x0002.0000 to 0x0003.FFF8 )
- What are the last 8 bytes used for? ( 0x0001.FFF8 to 0x0001.FFFF, or 0x0003.FFF8 to 0x0003.FFFF )
- I think it is not a good idea to use these bytes to store user data. But, what happens if I write data to these bytes?
Thanks and Best Regards!