Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3107: BSL invoke after program startup by enabling the BSL invoke pin

Part Number: MSPM0G3107
Other Parts Discussed in Thread: MSPM0G3507

Tool/software:

Hi team,

 

My account has several questions about BSL invoke.

  1. Is it possible to call the BSL after the program is started by enabling the BSL invoke pin?
  2. If the BSL invoke pin can be used to call the BSL after the program is started, please tell us how to read the BSL using the BSL_invoke pin below.
    1. When using MSPM0G3107 (package VSSOP20 (DGS20)), is 15 pin BSL invoke according to page 15 of mspm0g3107.pdf?
    2. Also, input NRST = low (less than 1s) to transition to BOOTRST state and if BSL_invoke is asserted at the timing when NRST is released, the BSL will start.
      Is my understanding correct ?

Thank you in advance.

Best regards,

Kenley