Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM263X: Multicore Debug causes Abort

Part Number: MCU-PLUS-SDK-AM263X

Tool/software:

I have been having issues debugging multi-core applications since I’ve been using AM263Px. The symptom is that if multiple cores run simultaneously with both cores attached. I am using SBL_NULL (not DEV_BOOT) on AM263Px Control Card Evaluation Module. The symptoms I see is an Abort Exception.

 

SDK Version:

mcu_plus_sdk_am263px_09_02_00_56

 

I created a thread here:

MCU-PLUS-SDK-AM263X: Data Abort Troubleshooting, Register Analysis - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

… but moved on to other work, never resolving the issue.

 

I also see related discussions:

(+) MCU-PLUS-SDK-AM273X: Unreliable debugging of multicore applications - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

(+) AM2634: Multicore FreeRTOS Empty Project Doesn't Work Correctly - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

(+) MCU-PLUS-SDK-AM263X: Multicore Debug Target Configuration/GEL File Clarification - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

 

I reviewed these, but I do not see a solution in those threads.

 

 

I am using example SDK project:

/ipc_spinlock_sharedmem_am263px-cc_system_freertos_nortos

… to demonstrate here.

  • Select System Project and click “Debug”

 

  • This triggers the following output in the Console:

 

Cortex_R5_0: GEL Output: Gel files loading on R5F0 Complete

Cortex_R5_0: GEL Output: ***OnTargetConnect() Launched***

 

Cortex_R5_0: GEL Output: AM263Px Initialization Scripts Launched.

Please Wait...

 

 

Cortex_R5_0: GEL Output: AM263Px_Cryst_Clock_Loss_Status() Launched

Cortex_R5_0: GEL Output: Crystal Clock present

Cortex_R5_0: GEL Output: AM263Px_SOP_Mode() Launched

Cortex_R5_0: GEL Output: SOP MODE = 0x00000003   

Cortex_R5_0: GEL Output:

 OSPI - 8S Functional boot mode

Cortex_R5_0: GEL Output: AM263Px_Read_Device_Type() Launched

Cortex_R5_0: GEL Output: EFuse Device Type Value = 0x000000AA   

Cortex_R5_0: GEL Output: AM263Px_dual_or_lockstep_mode() Launched

Cortex_R5_0: GEL Output: r5fss0 = 0x00000001   

Cortex_R5_0: GEL Output: r5fss1 = 0x00000000   

Cortex_R5_0: GEL Output:

 R5FSS0 is in Dual core mode

Cortex_R5_0: GEL Output:

 R5FSS1 is in Dual core mode

Cortex_R5_0: GEL Output: MSS_CTRL Control Registers Unlocked

Cortex_R5_0: GEL Output: MSS_TOP_RCM Control Registers Unlocked

Cortex_R5_0: GEL Output: MSS_RCM Control Registers Unlocked

Cortex_R5_0: GEL Output: MSS_IOMUX Control Registers Unlocked

Cortex_R5_0: GEL Output: TOP_CTRL Control Registers Unlocked

Cortex_R5_0: GEL Output:

 

*** R5FSS0 Reset DualCore ***

Cortex_R5_0: GEL Output:

 

***R5FSS1 Reset DualCore ***

Cortex_R5_0: GEL Output: R5F ROM Eclipse

Cortex_R5_0: GEL Output: R5FSS0_0 Released

Cortex_R5_0: GEL Output: R5FSS0_1 Released

Cortex_R5_0: GEL Output: R5FSS1_0 Released

Cortex_R5_0: GEL Output: R5FSS1_1 Released

Cortex_R5_0: GEL Output: L2 Mem Init Complete

Cortex_R5_0: GEL Output: MailBox Mem Init Complete

Cortex_R5_0: GEL Output: *********** R5FSS0/1 Dual Core mode Configured********

Cortex_R5_0: GEL Output: SYS_CLK DIVBY2

Cortex_R5_0: GEL Output: DPLL_CORE_HSDIV0_CLKOUT0 selected as CLK source for R5FSS & SYS CLKs

Cortex_R5_0: GEL Output:

 CLK Programmed R5F=400MHz and SYS_CLK=200MHz

Cortex_R5_0: GEL Output:

 

 *** Enabling Peripheral Clocks ***

Cortex_R5_0: GEL Output: Enabling RTI[0:3] Clocks

Cortex_R5_0: GEL Output: Enabling RTI_WDT[0:3] Clocks

Cortex_R5_0: GEL Output: Enabling UART[0:5]/LIN[0:5] Clocks

Cortex_R5_0: GEL Output: Enabling QSPI Clocks

Cortex_R5_0: GEL Output: Enabling I2C Clocks

Cortex_R5_0: GEL Output: Enabling TRACE Clocks

Cortex_R5_0: GEL Output: Enabling MCAN[0:3] Clocks

Cortex_R5_0: GEL Output: Enabling MMCSD Clocks

Cortex_R5_0: GEL Output: Enabling MCSPI[0:4] Clocks

Cortex_R5_0: GEL Output: Enabling CONTROLSS Clocks

Cortex_R5_0: GEL Output: Enabling CPTS Clocks

Cortex_R5_0: GEL Output: Enabling RGMI[5,50,250] Clocks

Cortex_R5_0: GEL Output: Enabling XTAL_TEMPSENSE_32K Clocks

Cortex_R5_0: GEL Output: Enabling XTAL_MMC_32K Clocks

Cortex_R5_0: GEL Output:

 

 ***All IP Clocks are Enabled***

 

Cortex_R5_0: AM263Px

Cortex_R5_0: Board Selected : CC

Cortex_R5_0: Part Selected : Standard

Cortex_R5_1: AM263Px

Cortex_R5_1: Board Selected : CC

Cortex_R5_1: Part Selected : Standard

 

3)

Eventually both cores are halted at main.

 

4)

I can run core r5fss0-0, and halt it while core r5fss0-1 is halted.

 

5)

I can run core r5fss0-1, and halt it while core r5fss0-0 is halted.

6)

However, when I run If I try to run simultaneously by starting core r5fss0-1, and then starting r5fss0-0, an abort occurs immediately on r5fss0-1.

 

Please advise.

  • Hey Tollman,

    So, I think this issue is occurring due to the fact that you are using SBL Null boot, but CCS is still initiating the OnTargetConnect() function and attempting to reconfigure the device as if in No-Boot mode.

    Can you navigate to C://ti/ccs12xx/ccs/ccs_base/emulation/gel/AM263Px/AM263Px.gel and comment out lines 78-103 as shown in the screenshot below and let me know your results after running?

    Thanks,

    Zackary Fleenor