Part Number: UNIFLASH
Other Parts Discussed in Thread: CC2340R5
Tool/software:
i'm using UniFlash 8.7.0 to generate "standalone" command-line packages for windows, linux, and macos....
all is well on windows and linux; and the generate .zip file has all the correct pieces for macos....
the "problem" is that macos has become stricter and stricter when running executables extracted from a .zip file from an unknown source....
my end-user (who will unzip a command-line package that i've prepared) will be hit with a flurry of messages that make it virtually impossible to proceed....
worse case, i can have my end-user simply download/install the uniflash .dmg file; but that diminishes somewhat my value in providing a pleasant OOB experience....
is there someone with "deep" knowledge of macos that could perhaps suggest a fix or workaround; as is, the standalone command-line package is basically useless....
for reference, i'm sitting on macos ventura 13.5; and i'm actually using uniflash with a CC2340R5 (though my issue is probably target independent)....