Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570_SAFETY_MCU_DEMOS: SAFETY_MCU

Part Number: TMS570_SAFETY_MCU_DEMOS
Other Parts Discussed in Thread: TMS570LC4357

Tool/software:

Hi team,

We need a SIL certified controller (SIL2/SIL3)  with below specification support

1. UART - 3x

2. SPI - 2x

3. GPIO - 10x

  • If possible , suggest

    low power consumption MCU

  • Hi Hithesh,

    Apologies for the delay in late response.

    All the Hercules series of controllers will support upto SIL3.

    We need a SIL certified controller (SIL2/SIL3)  with below specification support

    1. UART - 3x

    2. SPI - 2x

    3. GPIO - 10x

    Regarding 3 UART/SCI, most of the controllers will have only 2 UART/SCI.

    Only below couple of controllers have 4 UART/SCI.

    So, to satisfy these requirements either you should choose RM57Lx or TMS570LC4357 controllers.

    low power consumption MCU

    The typical CPU core power consumption for these devices is 260mA, and maximum is 420mA.

    For example, you can see the below graph:

    --
    Thanks & regards,
    Jagadish.