Part Number: LP-MSPM0G3507
Tool/software:
#include "ti_msp_dl_config.h"
int main(void)
{
SYSCFG_DL_init();
/* Enable TimerG interrupts on device */
NVIC_EnableIRQ(TIMER_0_INST_INT_IRQN);
/* Enable sleep on exit */
DL_SYSCTL_enableSleepOnExit();
/* Set LED to indicate Timer counter enable */
DL_GPIO_clearPins(
GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN | GPIO_LEDS_USER_TEST_PIN);
/* Start TimerG counter */
DL_TimerG_startCounter(TIMER_0_INST);
while (1) {
__WFI();
}
}
void TIMER_0_INST_IRQHandler(void)
{
switch (DL_TimerG_getPendingInterrupt(TIMER_0_INST)) {
case DL_TIMER_IIDX_ZERO:
/* Restart WWDT timer */
DL_WWDT_restart(WWDT0_INST);
/* Toggle LED to indicate WWDT reset */
DL_GPIO_togglePins(GPIO_LEDS_PORT,
GPIO_LEDS_USER_LED_1_PIN | GPIO_LEDS_USER_TEST_PIN);
break;
default:
break;
}
}
Hello, I encounter such errors when I change the period count without changing the WDT sample code at all. What is the solution or am I doing something wrong?