This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: AM2634 TCP maximum speed

Part Number: AM2634

Tool/software:

Hello expert,
I used enet_cpsw_tcpserver_am263x-lp_r5fss0-0_freertos_ti-arm-clang to test the maximum speed of TCP by sending data continuously, which is currently 200Mbps, but the cpu utilization is only 75%. What are the factors that limit the speed to continue to increase, I can continue to increase the TCP rate.
In addition, when will the MCU_SDK 10.0 version be released, thank you very much~.