Part Number: TIDEP-01032
Tool/software:
Dear Ti Experts
The TIDEP-01032 has been developed using Motors with Endat2.2. I would like to use Motor with HDSL in SYNC Mode. Could you give hints on the the changes needed.
I've looked at HDSL diagnostic SYNC implementation, It is not obvious to me the sections that need to be changed to enable PWM SYNCOUT instead of IEP1 sync
Also, I only need to run 1 motor at this stage.
Thank you
Alan I