Part Number: AM2634
Other Parts Discussed in Thread: DP83869, LP-AM263, DP83869EVM
Tool/software:
Hello,
We are trying to configure DP83869 in 1000Base-FX mode, that is connected to AM2634 MCU.
The circuit is based on both evaluation boards: LP-AM263 and DP83869EVM.
More precisely, almost the whole our scematic is the same as LP-AM263's one, but we added connection to a SFP module, the way it is connected on DP83869EVM.
The problem is that we are unable to switch DP83869 to work in fiber mode (neither via the strapping pins nor via the MDIO interface) - it always stays in copper mode.
Regarding the software part - it is based on the example project "Enet Lwip TCP Server Example on CPSW" from AM2634's SDK.
It looks like the library tries to force DP83869 all the time in copper mode.
What is the proper way to configure DP83869 in fiber mode, using the AM2634's SDK?
Best regards,
V. Dimov