Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1305: Build an MSPM0 project using bx-docker in linux ubuntu and iar build tools

Part Number: MSPM0L1305
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

We are still looking at how to build the TI project through the command line using bx-docker and ran into the following issue, It builds in windows using the following command  iarbuild c:\projectReset\Project-Reset-4000-Series.ewp -build Debug -parallel 4 -varfile c:\projectReset\Project-Reset-4000-Series.custom_argvars.

 

This is the output I get running the following command in bx-docker

 

docker run --rm -v LMS2:/usr/local/etc/IARSystems -v $PWD:/build iarsystems/bxarm:9.50.2 /opt/iarsystems/bxarm/common/bin/iarbuild Project-Reset-4000-Series.ewp -build Debug -parallel 4 -varfile Project-Reset-4000-Series.custom_argvars

 

     IAR Command Line Build Utility V9.3.2.390

     Copyright 2002-2023 IAR Systems AB.

 

 

Project-Reset-4000-Series - Debug

Reading project nodes...

 

Variable expansion failed.

  Offending text: "$MSPM0_SDK_INSTALL_DIR$/source/third_party/CMSIS/Core/Include/"

  Partial command line: ""$TOOLKIT_DIR$/bin/iccarm" "/build/EEPROM_EMULATION/eeprom_emulation_type_a.c" "-D" "__MSPM0L1305__" "-D" "BUILD_NUM_MSB=0" "-D" "MAJOR_SW_REV_LEVEL=0" "-D" "BUILD_NUM_LSB=1" "-o" "/build/Debug/Obj/$ROOT_REL_PATH$" "--no_unroll" "--no_inline" "--no_tbaa" "--no_scheduling" "--debug" "--endian=little" "--cpu=Cortex-M0+" "--debug" "--silent" "-e" "--aeabi" "--thumb" "--diag_suppress=Pa050" "-e" "--fpu=None" "--dlib_config" "$TOOLKIT_DIR$/inc/c/DLib_Config_Normal.h" "-I" "$PROJ_DIR$/" "-I" "$MSPM0_SDK_INSTALL_DIR$/source/third_party/CMSIS/Core/Include/" "-I" "$MSPM0_SDK_INSTALL_DIR$/source/" "-I" "$MSPM0_SDK_INSTALL_DIR$/source/ti/driverlib/" "-I" "$PROJ_DIR$/Core/Src/" "-I" "$PROJ_DIR$/Core/Inc/" "-I" "$PROJ_DIR$/EEPROM_EMULATION/" "-Om" "--vla" "

Failed to generate node description for C/C++ Compiler tool and file(s): eeprom_emulation_type_a.o

Failed to generate build node descriptions

Reading project nodes failed.

 

 

We have the following setup in the following file /ti/mspm0_sdk_2_01_00_03/tools/iar# nano MSPM0_SDK.custom_argvars

 

 

 

 

<?xml version="1.0" encoding="iso-8859-1"?>

 

<iarUserArgVars>

  <group active="true" name="MSPM0_SDK">

    <variable>

      <name>SYSCONFIG_ROOT</name>

      <value>build/ti/sysconfig_1.20.0</value>

    </variable>

    <variable>

      <name>MSPM0_SDK_INSTALL_DIR</name>

      <value>build/ti/mspm0_sdk_2_01_00_03</value>

    </variable>

    <variable>

      <name>MSP_SDK_INSTALL_DIR</name>

      <value>build/ti/mspm0_sdk_2_01_00_03</value>

    </variable>

    <variable>

      <name>EXAMPLE_ROOT</name>

      <value>build/ti/mspm0_sdk_2_01_00_03/tools/iar</value>

    </variable>

  </group>

</iarUserArgVars>