This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: There is something unclear about TRM "9.2.1.1.1 GICSS Features"

Part Number: AM2431

Tool/software:

The TRM refers to spruim2g.pdf.

TRM "9.2.1.1.1 GICSS Features" states "Programmable, affinity-based interrupt routing."

Regarding the above sentence, I don't understand what "affinity-based interrupt routing" means.

I would like to know more about "affinity-based interrupt routing."

Thank you in advance.

  • Hello 

    I would like to know more about "affinity-based interrupt routing."

    Thanks for your query.

    The GIC-500 interrupt controller provides registers for managing interrupt sources, interrupt behavior, and interrupt routing to one or more cores. 

    It supports Programmable interrupt routing that is based on affinity. It has 1-32 Number of affinity-level 1 clusters.

    The ARM architecture defines a register in a core that identifies the logical address of the core in the system. This register, which is known as the Multiprocessor Affinity Register (MPIDR), has a hierarchical format. Each level of the hierarchy is known as an affinity level, with the highest affinity levels specified first:

    • For an ARMv7 processor, the MPIDR defines three levels of affinity, with an implicit affinity level 3 value of 0.

    • For an ARMv8 processor, the MPIDR defines four levels of affinity.

    For more information on the above features, please refer to ARM GIC-500 interrupt controller TRM.

    Please refer About-GIC-500-controller. 

    Regards,

    Tushar