Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
I have a CCS project built based on application note spna192. I get a file-erase error when attempting to run the application. Oddly, the application loads and runs peroperly, but it is unable to erase flash. I tried erasing the flash using "all sectors" in the project properties but see non-FFFFFFFF addresses throughout the remaining flash address space. This behaves in a similar fashion on a known good Launchpad and a production board. I suspect that I have a configuration error that is causing this problem. I tried invalidating the icashe and calling Fapi_flushPipeline() with no success.
e.g. FFFF FFFF FF7F FFFF FFFF FFFF FFFF FFFF FFCB FEFF FFFF FFFF FFFF
FFFF FFBF FFFF FFBE FBFF FFFF FFFF FFFF FFFF FFDF FFFF FFFF FFFF
FFFE FFFF FF5F 7FFF FFFF FFFF FF7B EFFF FFFF FFFF FFFF FFFF FFF7
FFFF FFFF FFFF FFFB FFFF FFB7 DFFF FFFF FFFF BFFF FFEF FFB6 D9FF
FFFF FFFF FFFF FFFF FFF6 FDFF FFFF FFEF FFFF FFFF FF7F FFFF FFB7
DFFF
Any help is appreciated.
uint32_t Fapi_BlockErase( uint32_t ulAddr, uint32_t Size)
{
uint8_t i=0U;
uint8_t ucStartBank;
uint8_t ucEndBank;
uint8_t ucStartSector;
uint8_t ucEndSector;
uint32_t EndAddr;
uint32_t status;
#if 1
EndAddr = ulAddr + Size;
for(i = 0; i < NUMBEROFSECTORS; i++)
{
if((ulAddr >= (uint32_t)(flash_sector[i].start)) && (ulAddr < ((uint32_t)flash_sector[i].start + flash_sector[i].length)))
{
ucStartBank = flash_sector[i].bankNumber;
ucStartSector = i;
break;
}
}
for(i = ucStartSector; i < NUMBEROFSECTORS; i++)
{
if(EndAddr <= (((uint32_t)flash_sector[i].start) + flash_sector[i].length))
{
ucEndBank = flash_sector[i].bankNumber;
ucEndSector = i;
break;
}
}
//API Rev2.01
status = Fapi_initializeFlashBanks((uint32_t)SYS_CLK_FREQ);
if(status == Fapi_Status_Success)
{
status = Fapi_enableAutoEccCalculation();
for(i = ucStartBank; i < (ucEndBank + 1); i++)
{
if(status != Fapi_Status_Success)
{
break;
}
status = Fapi_setActiveFlashBank((Fapi_FlashBankType)i);
if(status != Fapi_Status_Success)
{
break;
}
//API Rev2.01
status = Fapi_enableMainBankSectors(0xFFFF);
if(status != Fapi_Status_Success)
{
break;
}
while(FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady);
}
for(i=ucStartSector; i<(ucEndSector+1); i++)
{
Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, flash_sector[i].start);
if(status != Fapi_Status_Success)
{
break;
}
while(FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy);
while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
}
}
status |= Flash_Erase_Check( ulAddr, Size);
return (status);
}
uint32_t Flash_Erase_Check(uint32_t Start_Address, uint32_t Bytes)
{
uint32_t error = ERASE_NO_ERR;
register uint32_t *dst1 = (uint32_t *) Start_Address;
register uint32_t bytes = Bytes;
_iCacheInvalidate_();
Fapi_flushPipeline(); /* flush cache */
while(bytes > 0U)
{
if(*dst1++ != 0xFFFFFFFFU)
{
error = ERASE_ERR;
break;
}
bytes -= 0x4U;
}
return error;
}