Part Number: MSPM0L1228
Tool/software:
Hi,
As the MSPM0L1228 flash memory description,
Up to 100000 program/erase cycles on the lower 32KB of the flash memory, with up to 10000 program/erase cycles on the remaining flash memory
If the main flash is split into two banks, Do the program/erase cycles mentioned above apply to each bank individually, or to the two banks combined?
For ex,
Bank0: 100000 and 10000, Bank1: 100000 and 10000
or
Bank0 + Bank1: 100000 and 10000
Best Regards!