This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: There is something unclear about TRM "12.1.2.4.3.3 Interrupt Status and Clear (per Bit)"

Part Number: AM2431


Tool/software:

The TRM refers to spruim2g.pdf.

TRM section "12.1.2.4.3.3 Interrupt Status and Clear (per Bit)" states "The UART module is capable of supporting a 9-bit mode that is not shown in the diagram."

However, TRM section "12.1.5.1.4 UART Not Supported Features" states "9-bit mode."

Does the UART support 9-bit mode, or not?

Thank you in advance for your help.

  • Hello ,

    I have already working on your threads for the yesterday assigned  threads and you may get a delayed reply to this thread.

    Please consolidate all threads into one thread thread . So, that all our engineers can reply in the same thread, which will reduce the burden on us and you as well.

    Regards,

    Anil.