This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: I would like to confirm "modem mode" in TRM "12.1.5.4.4.1.1 Module Power Saving"

Part Number: AM2431


Tool/software:

The TRM refers to spruim2g.pdf.

TRM section "12.1.5.4.4.1.1 Module Power Saving" states that "Sleep mode is a good way to lower UART power consumption, but this state can be achieved only when the UART is set to modem mode."
I would like to know what "modem mode" in the above sentence means.

Thank you in advance for your help.

  • Hello 

    Thank you for the query and your inputs to improve the SOC collaterals.

    I see the following threads assigned to me and i suspect you may have additional queries (threads) that may be answered by other members supporting customers.

    Could you please consolidate all the queries into a single thread on a day basis ( i see the difference between thread are a few minutes) or at the least 5..6 queries into a single thread or queries related to a specific section or chapter in the TRM into a single thread, it would be easy for us to track and reply.

    More threads could possibly result in delayed response or missed response compared to providing response for consolidated threads.

    I will close this thread. Please start a new thread (consolidate multiple threads into a single thread) to provide focused support.

    Please expect delay in response since as i will have to check internally with multiple teams to get the queries answered.

    Regards,

    Sreenivasa