Part Number: MSPM0G1107
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Madhurya,
I want to add to the question which was sent by us with the same mail subject.
We have the mspm01107 embedded on our board.
We can measure the current to the m0 by placing a small resistor to the vdd of the m0.
- The current drawn by an empty m0 (erased) is very low < 1uA.
- The current drawn by an m0 hold in reset is 500uA
- The current drawn by a project which has 25 pins set to input no pull is 1.9mA. All not used pins are also set to input no pull.
What are we doing wrong?
}
Content: ti_msp_dl_config.c