This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3107-Q1: Absolute ratings section for datasheet (7.1) supported diode current

Part Number: MSPM0G3107-Q1

Tool/software:

Hi,

I'm looking for clarification of the specification pointed to in the section shown below.

Is the diode current referring to the pin protection diodes and the current is the maximum allowed before the device is damaged?

If so, does that allow me to connect a 10V supply (for example), through a 10k Ohm current limiting resistor to a device input?

thanks,

dave