Part Number: MSPM0G3507
Other Parts Discussed in Thread: DRV8316
Tool/software:
Hi,
I am using mspm0_sdk_2_02_00_05 with DRV8316 to develop FOC motor control project.
For the following function in file "focHALInterface.c",
void HAL_SelectShuntMeasure(HAL_MEASURE_MOTOR_INPUTS_T *pMotorInputs)
{
HAL_MEASURE_CURRENT_T *pCurrent = &(pMotorInputs->current);
MC_PHASE_TYPES maxDutyPhase = *(pCurrent->pMaxDutyPhase);
#ifdef CURRENT_THREE_SHUNT_DYNAMIC
if(maxDutyPhase != pCurrent->prevMaxDutyPhase &&
pCurrent->flags.b.threeShuntDynamic)
{
/* Max duty phase has changed and dynamic update on 3
* shunt is enabled */
switch(maxDutyPhase)
{
case PHASE_A:
pCurrent->currentShunt = CURRENT_TWO_SHUNT_B_C;
break;
case PHASE_B:
pCurrent->currentShunt = CURRENT_TWO_SHUNT_A_C;
break;
case PHASE_C:
pCurrent->currentShunt = CURRENT_TWO_SHUNT_A_B;
break;
case PHASE_INVALID:
pCurrent->currentShunt = pCurrent->currentShuntSet;
break;
}
HAL_SetPhaseCurrentChannels(pMotorInputs);
}
#endif
}
I think
#ifdef CURRENT_THREE_SHUNT_DYNAMIC
should be
#ifdef __CURRENT_THREE_SHUNT_DYNAMIC
It is a typo, right?
Robert.