This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Trip Zone on TZ3 N2HET1[10]:

Part Number: TMS570LS1224

Tool/software:

Hi,

I'm referring to my product code, a 5 years back code basically.

I see in my product schematics N2HET1[10]/TZ3 i.e Trip zone 3 is connected to one of the device

But, when i refer in code i see pwmStart (hetRAM1, 1U); corresponds to TZ3.

I'm not able to corelate is that parameter 1U corresponds to PWM1?

If so, which halogen generated file, where i can find information where PWM1 is muxed with TZ3?

Note:- At present we don't have halogen settings, which was done 5 years back.