Part Number: MSPM0G3107
Other Parts Discussed in Thread: MSPM0G3507, LP-MSPM0G3507, UNIFLASH
Tool/software:
Refer to bsl_software_invoke_app_demo_uart_LP_MSPM0G3507_nortos_ticlang, we want to duplicate the same method to
enter BSL mode by invokeBSLAsm() on G3107. But MCU will always reset on G3107 (can not stay in BSL "wait for command" state as illustration).
I also try DL_SYSCTL_resetDevice(DL_SYSCTL_RESET_BOOTLOADER_ENTRY), but not work as well.
Please help to advise the way to enter BSL mode on G3107 by software invoke.
__STATIC_INLINE void invokeBSLAsm(void)
{
/* Erase SRAM completely before jumping to BSL */
__asm(
#if defined(__GNUC__)
".syntax unified\n" /* Load SRAMFLASH register*/
#endif
"ldr r4, = 0x41C40018\n" /* Load SRAMFLASH register*/
"ldr r4, [r4]\n"
"ldr r1, = 0x03FF0000\n" /* SRAMFLASH.SRAM_SZ mask */
"ands r4, r1\n" /* Get SRAMFLASH.SRAM_SZ */
"lsrs r4, r4, #6\n" /* SRAMFLASH.SRAM_SZ to kB */
"ldr r1, = 0x20300000\n" /* Start of ECC-code */
"adds r2, r4, r1\n" /* End of ECC-code */
"movs r3, #0\n"
"init_ecc_loop: \n" /* Loop to clear ECC-code */
"str r3, [r1]\n"
"adds r1, r1, #4\n"
"cmp r1, r2\n"
"blo init_ecc_loop\n"
"ldr r1, = 0x20200000\n" /* Start of NON-ECC-data */
"adds r2, r4, r1\n" /* End of NON-ECC-data */
"movs r3, #0\n"
"init_data_loop:\n" /* Loop to clear ECC-data */
"str r3, [r1]\n"
"adds r1, r1, #4\n"
"cmp r1, r2\n"
"blo init_data_loop\n"
/* Force a reset calling BSL after clearing SRAM */
"str %[resetLvlVal], [%[resetLvlAddr], #0x00]\n"
"str %[resetCmdVal], [%[resetCmdAddr], #0x00]"
: /* No outputs */
: [ resetLvlAddr ] "r"(&SYSCTL->SOCLOCK.RESETLEVEL),
[ resetLvlVal ] "r"(DL_SYSCTL_RESET_BOOTLOADER_ENTRY),
[ resetCmdAddr ] "r"(&SYSCTL->SOCLOCK.RESETCMD),
[ resetCmdVal ] "r"(
SYSCTL_RESETCMD_KEY_VALUE | SYSCTL_RESETCMD_GO_TRUE)
: "r1", "r2", "r3", "r4");
}