Part Number: EK-TM4C1294XL
Tool/software:
Good morning
We've been using two variants of the EK-TM4C1294XL LaunchPad beds for a few years now in development.
The first uses the Ethernet connection to read commands from the host then stream data from eight input lines (ports) back to the host. The port connections are coming from the BoosterPack headers.
The second controls our processor unit using most of the port lines on the 99 pin (breadboard) edge connector. This variant does not use an Ethernet connections.
We will be programming both variants using the DEBUG interface and supplying our own 3.3V power supply.
Now we are preparing to mount the required circuitry to the layout of the two boards. Could you please let us know which components from the LaunchPad unit will be required for each purpose? I'm guessing the complete package will not be required in the end.
Your assistance is greatly appreciated. Nice little board.
Byron Blue
Hardware and software engineering
MAQ Sonar