Part Number: RM57L843
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello,
I´ve used Uniflash application to create a standalone command line package (zip) for the XDS100 v3.
On another PC, I ran "one_time_setup.bat" and then "dslite.bat" and got the following error message:
"Connecting...
fatal: IcePick: Error connecting to the target: (Error -717 @ 0x0) Required dynamic library jscserdesv3 could not be located. The library isn't on the search path. (Emulation package 12.7.0.00130)
Failed: Operation was aborted on 'CortexR5'"
I´ve installed "ti_emupack_setup_9.2.0.00002_win_64" and the error went away (solved the problem).
Wouldn´t the standalone command line zip package be enough? Why did I have to install the emupack?
Regards,