Part Number: MSPM0G3107
Tool/software:
Hi team,
Due to the pin setting, it seems difficult to implement ROSC (oscillator frequency compensation), so let me check the following two points.
(1) Are there any disadvantages to not using ROSC? I am aware that ROSC improves the accuracy of SYSOSC and has an accuracy of -2.7%~2.3% even if it is not implemented, is it correct?
(2) I would like to use the ROSC pin as an SPI (CS0), but in that case, are there any side effects on SYSOSC? Is it okay to understand that it is simply that the accuracy correction of SYSOSC is not included?
Thank you,
Kenley