Part Number: MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3106,
Tool/software:
Hi
I am using the MSPM0G3106/MSPM0G3507 for a UART DMA communication running at the following configuration.
Baud rate - 2mbps
CPU clock - 80Mhz
MCLK - 80Mhz
ULPCLK - 40Mhz ( max possible as per TRM )
UART0 ( Power Domain 0) being used which refers to ULPCLK at 40Mhz ( max) as the BUSCLK for its operation. DMA is used for RX and TX with the Triggers Set to transfer to and from RX/TX FIFOs. DMA ( Power Domain 1 ).
Problem Statement:
We are a TX Task running at 1ms , which creates packets of max 130 bytes at a time which will be the source buffer for the DMA to push to the UART TX FIFO. With an Internal Loopback enabled , we are observing random 1 or 2 bytes missing from the Packet transmitted. we have validated the packet structure till the buffer is given for UART DMA transaction, so the issue has to be the UART/DMA layer itself.
Observations :
1. The same code with the MCLK and CPU CLOCK set to 40Mhz , along with ULPCLK also at 40Mhz seems to be not giving the issue.
2. On a launchpad ,the same test conducted by using UART3 (PD1) instead of UART0(PD0) there by using the MCLK 80Mhz for UART3(PD1) - this setup is also working with the missing of bytes.
Is there any recommendations for using UART0 DMA with ULPCLK -40Mhz , MCLK - 80Mhz , CPU CLOCK - 80Mhz for attaining stability ?
Please find the code snippet for the configurations used when the issue is observed :
Clock Configurations ( SYS PLL) :
static const DL_SYSCTL_SYSPLLConfig gSYSPLLConfig = {
.inputFreq = DL_SYSCTL_SYSPLL_INPUT_FREQ_16_32_MHZ,
.rDivClk2x = 0,
.rDivClk1 = 0,
.rDivClk0 = 0,
.enableCLK2x = DL_SYSCTL_SYSPLL_CLK2X_DISABLE,
.enableCLK1 = DL_SYSCTL_SYSPLL_CLK1_ENABLE,
.enableCLK0 = DL_SYSCTL_SYSPLL_CLK0_ENABLE,
.sysPLLMCLK = DL_SYSCTL_SYSPLL_MCLK_CLK0,
.sysPLLRef = DL_SYSCTL_SYSPLL_REF_SYSOSC,
.qDiv = 9,
.pDiv = DL_SYSCTL_SYSPLL_PDIV_2
};
DL_SYSCTL_setSYSOSCFreq(DL_SYSCTL_SYSOSC_FREQ_BASE);
DL_SYSCTL_configSYSPLL((DL_SYSCTL_SYSPLLConfig *) &gSYSPLLConfig);
DL_SYSCTL_setMCLKSource(SYSOSC, HSCLK, DL_SYSCTL_HSCLK_SOURCE_SYSPLL);
DL_SYSCTL_setULPCLKDivider(DL_SYSCTL_ULPCLK_DIV_2);
//Low Power Mode is configured to be SLEEP0
DL_SYSCTL_setBORThreshold(DL_SYSCTL_BOR_THRESHOLD_LEVEL_0);
DL_SYSCTL_setFlashWaitState(DL_SYSCTL_FLASH_WAIT_STATE_2);
UART0 & DMA configurations:
DL_UART_Main_setOversampling(UART_INST, DL_UART_OVERSAMPLING_RATE_16X);
DL_UART_Main_setBaudRateDivisor(UART_INST, UART_IBRD_40_MHZ_2000000_BAUD, UART_FBRD_40_MHZ_2000000_BAUD);
DL_UART_Main_enableDMAReceiveEvent(UART_INST, DL_UART_DMA_INTERRUPT_RX);
DL_UART_Main_enableDMATransmitEvent(UART_INST);
/* Configure FIFOs */
DL_UART_Main_enableFIFOs(UART_INST);
DL_UART_Main_setRXFIFOThreshold(UART_INST, DL_UART_RX_FIFO_LEVEL_ONE_ENTRY);
DL_UART_Main_setTXFIFOThreshold(UART_INST, DL_UART_TX_FIFO_LEVEL_ONE_ENTRY);
/* Configuration for UART 0 Peripheral */
static const DL_UART_Main_ClockConfig gUART_ClockConfig = {
.clockSel = DL_UART_MAIN_CLOCK_BUSCLK,
.divideRatio = DL_UART_MAIN_CLOCK_DIVIDE_RATIO_1
};
static const DL_UART_Main_Config gUART_Config = {
.mode = DL_UART_MAIN_MODE_NORMAL,
.direction = DL_UART_MAIN_DIRECTION_TX_RX,
.flowControl = DL_UART_MAIN_FLOW_CONTROL_NONE,
.parity = DL_UART_MAIN_PARITY_NONE,
.wordLength = DL_UART_MAIN_WORD_LENGTH_8_BITS,
.stopBits = DL_UART_MAIN_STOP_BITS_ONE
};
/*configuration for DMA TX channel - Channel 1*/
static const DL_DMA_Config gDMA_CH1Config = {
.transferMode = DL_DMA_SINGLE_TRANSFER_MODE,
.extendedMode = DL_DMA_NORMAL_MODE,
.destIncrement = DL_DMA_ADDR_UNCHANGED,
.srcIncrement = DL_DMA_ADDR_INCREMENT,
.destWidth = DL_DMA_WIDTH_BYTE,
.srcWidth = DL_DMA_WIDTH_BYTE,
.trigger = UART_INST_DMA_TRIGGER_1,
.triggerType = DL_DMA_TRIGGER_TYPE_EXTERNAL,
};
/*configuration for DMA RX channel - Channel 0*/
static const DL_DMA_Config gDMA_CH0Config = {
.transferMode = DL_DMA_FULL_CH_REPEAT_SINGLE_TRANSFER_MODE,
.extendedMode = DL_DMA_NORMAL_MODE,
.destIncrement = DL_DMA_ADDR_INCREMENT,
.srcIncrement = DL_DMA_ADDR_UNCHANGED,
.destWidth = DL_DMA_WIDTH_BYTE,
.srcWidth = DL_DMA_WIDTH_BYTE,
.trigger = UART_INST_DMA_TRIGGER_0,
.triggerType = DL_DMA_TRIGGER_TYPE_EXTERNAL,
};