Part Number: LP-AM243
Tool/software:
Dear specialists,
I have a AM243X-LP demo-board. I successfully did "Flash SOC Initialization binary" on the AM243X-LP demo-board.
According to AM243X MCU+ SDK 10.00.00 "Getting Started" chapter's "EVM Setup" section, the next step is "SOC Initialization Using CCS Scripting".
I set the path to the SDK. The next step is to "Create Target Configuration" and "Launch Selected Configuration".
I have problem on the step "Create Target Configuration". I follow the instruction to use CCS pull-down command "view" and then click the "Target Configuration" to open a Target Configuration window.
Inside the Target Configuration window, the "User Defined" folder doesn't have any ccxml file in it (but, the SDK 10 shows a ccxml file in it).
How do I do in order to "Create" a target configuration ccxml file inside that folder?
Please help.
Thank you very much.
Best Regards, JasonChiu.