Part Number: MSP432E401Y
Tool/software:
Hello
We have been developing a couple of applications, the applications have embedded CRC in them for build and target load verifications.
We found one designer was using revision 3.62.1.15 of the XDCTools and the other revision 3.61.01.25.
These different revisions when used to no surprise result in an application with two different CRCs.
I have version 3.61.01.25 which is bundled with the simplelink_msp432e4_sdk_4_20_00_12 installer.
And version 3.62.1.15 which is bundled with CCS version 10.4.0.00006.
Would it be possible to clarify what revision of this toolset should be used and why?
Thanks In Advance
Perry