Part Number: AM2434
Other Parts Discussed in Thread: LMK1C1104
Tool/software:
Hi,
There is the description “A DC steady-state condition is not allowed on MCU_OSC0_XI when the oscillator is powered up.” at 6.10.4.1.2 MCU_OSC0 LVCMOS Digital Clock Source in the datasheet.
Why is inversion logic necessary?
Is there a problem with C-cut (C-coupling) instead of inverting logic?
On the EVM, the output of the CDCLVC1310RHBR is input directly to the AM2434.
Is this because no DC is applied from the output of CDCLVC1310RHBR ?
In the above case, if the clock buffer and oscillator outputs are not DC steady-state,
Is it OK to input directly from the clock IC to the AM2434?
Thanks and regards,
Hideaki