Part Number: MSPM0G3107
Other Parts Discussed in Thread: SYSCONFIG, LP-MSPM0L1306
Tool/software:
Hi
I'm using the MSPM0G3107 chip and I need to use MCAN to communicate several chips from different manufacturers. I'm using the TCAN1057A chip, however I can't get any output. I'm measuring with a direct logic analyzer on pins PA12 and PA13 but I'm not getting any output. My goal is to make it work without an external crystal, so I'm using the example "mcan_loopback_LP_MGPM0G3507_nortos_ticlang" and I've changed the input to "SYSPLLCLK1".
Settings:
SYSCTL -> Use Clock Tree (Disable)
SYSCTL->Clock Configuration->SYSPLL->Enable SYSPLLCLK1 (Enable)
SYSCTL->CANCLK->CANCLK Source (SYSPLLCLK1)
I haven't touched the rest of the settings. What do I need to configure for it to work?
Note: If I leave the "Use Clock Tree" setting active, the MSPM0 does lose when setting the Clock.
CSS: 12.8.0.00012
Compiler: TI Clang V3.2.2.LTS
MSPM0 SDK: 2.2.0.05
SysConfig: 1.21.0