This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: MSPM0 Connection

Part Number: TMDSEMU110-U

Tool/software:

Hi team,

Customer would like to ask about the connection between TMDESEMU110-U and the prototype board (MSPM0).
If the MSPM0 is not powered by the debug probe, and the MSPM0 is operated by an external input power supply (1.9V), is it sufficient to connect only SWDIO/SWCLK as shown in Figure 1?
Also, is it correct to type 1.9 in Enter voltage in the capture screen below (Figure 2)?

Fig.1.

Fig.2.

Thank you,

Kenley