Tool/software:
Hi
AM243 customer board
Senario:
Primary boot: ospi
Backup: uart boot
With uart connected to PC, Power off and power on, primary boot was jumped and go into backup boot.
Without uart connected to PC, power off and power on, ospi boot can succeed.
Reproduction way:
Power off and power on in seconds, 100% reproduce into uart boot.
Power off, wait one minute or longer, power on, boot succeed
HW change:
With this, there is no problem:
With this, there is problem.
Customer need:
Help to analyze if there is HW issue, if yes, change to previous version, any risk left?
Thanks
Regards
Zekun