Other Parts Discussed in Thread: SYSCONFIG
Hi
We're using SPI filters (Ferrite-Bead + Capacitor) on both SPI1 and SPI3 to communicate with UCC5880.
The circuit on each line looks like this:

We observe data corruption on SPI3 but not on SPI1. knowing that both circuits and loads are identical.
This screenshot from the datasheet shows a maximum load capacitance of 24pF - Could that explain the behavior ? but why not on SPI1 ?

Clock :4MHz
Thanks
Yassine