Part Number: MSPM0G3507
Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
Hello All,
Currently I am trying to flash application.hex file through BSL invocation for target microcontroller.
I have connected PA10,PA11,PA18, RESET, VCC and GND pins to the target PCB., apart from this I have connected SWCLK and SWDIO pins also at J101 and J101 is made open from on chip MSPM03507
through the TI GUI (MSPM0_BSL_GUI) which is present in SDK, I am able to flash application.txt file through BSL -> Successful
But with Uniflash, not able to flash.
I have selected MSPMG3507 in bootloader and given demo application and default password files.COM ports are properly set to relevant ports.
but I get below error while trying through Uniflash