Part Number: EK-TM4C1294XL
Tool/software:
Hi,
I have the below code. The expectation is that when I press the User Switch2, it should print out the message "IntHandlerPortJ User Switch 2..". However, the interrupt handler is never called. I even put a breakpoint on the default interrupt handler and even that is not called. Not sure what is wrong.
-------
void IntHandlerPortJ(void)
{
GPIOIntClear(GPIO_PORTJ_BASE, GPIO_INT_PIN_1);
Debugprintf("IntHandlerPortJ User Switch 2..");
}
void PortJ_Init(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOJ));
GPIOPinTypeGPIOInput(GPIO_PORTJ_BASE, GPIO_PIN_1);
GPIOPadConfigSet(GPIO_PORTJ_BASE, GPIO_PIN_1, GPIO_STRENGTH_10MA, GPIO_PIN_TYPE_STD_WPU);
GPIOIntTypeSet(GPIO_PORTJ_BASE, GPIO_PIN_1, GPIO_FALLING_EDGE | GPIO_DISCRETE_INT);
GPIOIntRegisterPin(GPIO_PORTJ_BASE, GPIO_PIN_1, IntHandlerPortJ);
GPIOIntEnable(GPIO_PORTJ_BASE, GPIO_INT_PIN_1);
}
int main(void)
{
InitSystemClock();
PortJ_Init();
while (1);
return 0;
}