Part Number: MSPM0G3507
Tool/software:
Hello.
I can get a single ADC to trigger from an external GPIO rising edge.
If I then add the second ADC there is NO option to select trigger from the same GPIO....but I can see the other ADC trigger for ADC0.
In other words, I want both ADCs to trigger from the same GPIO..I do not think this is possible.
Regards
Phil