This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM: printf() does not work!!!

Part Number: TM4C123GH6PM


Tool/software:

Hello Everyone,

I have a really frustrating simple problem. PRINTF() does NOT WORK!!!

I have two projects, project_A and project_B. I want project_A printf() to work and send text to the console. 

The source files are the same,

//This does not work.

#include <stdio.h>

int main(void) {
    printf("Hello");
    fflush (stdout);
    printf(" World!");
    fflush (stdout);

    return 0;
}

//This does work.

#include <stdio.h>

int main(void) {
	printf("Hello");
	fflush (stdout);
	printf(" World!");
	fflush (stdout);
	
	return 0;
}

The linker command files are the same,

/******************************************************************************
 *
 * Default Linker Command file for the Texas Instruments TM4C123GH6PM
 *
 * This is derived from revision 15071 of the TivaWare Library.
 *
 *****************************************************************************/
//This does not work.
--retain=g_pfnVectors

MEMORY
{
    FLASH (RX) : origin = 0x00000000, length = 0x00040000
    SRAM (RWX) : origin = 0x20000000, length = 0x00008000
}

/* The following command line options are set as part of the CCS project.    */
/* If you are building using the command line, or for some reason want to    */
/* define them here, you can uncomment and modify these lines as needed.     */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone.              */
/*                                                                           */
/* --heap_size=0                                                             */
/* --stack_size=256                                                          */
/* --library=rtsv7M4_T_le_eabi.lib                                           */

/* Section allocation in memory */

SECTIONS
{
    .intvecs:   > 0x00000000
    .text   :   > FLASH
    .const  :   > FLASH
    .cinit  :   > FLASH
    .pinit  :   > FLASH
    .init_array : > FLASH

    .vtable :   > 0x20000000
    .data   :   > SRAM
    .bss    :   > SRAM
    .sysmem :   > SRAM
    .stack  :   > SRAM
}

__STACK_TOP = __stack + 512;

/******************************************************************************
 *
 * Default Linker Command file for the Texas Instruments TM4C123GH6PM
 *
 * This is derived from revision 15071 of the TivaWare Library.
 *
 *****************************************************************************/
//This does work.
--retain=g_pfnVectors

MEMORY
{
    FLASH (RX) : origin = 0x00000000, length = 0x00040000
    SRAM (RWX) : origin = 0x20000000, length = 0x00008000
}

/* The following command line options are set as part of the CCS project.    */
/* If you are building using the command line, or for some reason want to    */
/* define them here, you can uncomment and modify these lines as needed.     */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone.              */
/*                                                                           */
/* --heap_size=0                                                             */
/* --stack_size=256                                                          */
/* --library=rtsv7M4_T_le_eabi.lib                                           */

/* Section allocation in memory */

SECTIONS
{
    .intvecs:   > 0x00000000
    .text   :   > FLASH
    .const  :   > FLASH
    .cinit  :   > FLASH
    .pinit  :   > FLASH
    .init_array : > FLASH

    .vtable :   > 0x20000000
    .data   :   > SRAM
    .bss    :   > SRAM
    .sysmem :   > SRAM
    .stack  :   > SRAM
}

__STACK_TOP = __stack + 512;

I have tried to make the project settings match as close as possible.

The projects are attached.

Thanks,

Allan

printf.zip