Part Number: AM2434
Tool/software:
Hello Team,
My company are developing industry communication base on Ethernet/IP slave within AM2434, but there are some question request support
1. the max node can be connected with one line (daisy chain topology)?, the protocol stack support 100 node?
2. the Ethernet/IP work on GMII mode up to 100Mbps, not 1Gbps?
3.the max latency between two node when setup 100 node?
My team had took some days to discuss the details, the scan time(2ms) per cycle up to 100 node is critical for us product, we must make decision the Ethernet/IP can work or not soon, or we need switch to EtherCat.
Expert to your reply soon, thanks very much!