Part Number: MSPM0G3507
Tool/software:
Hello,
I'm trying to understand ADC HW Averaging of MSPM0G3507 a little better.
I'm trying to sample a signal at 20kHz frequency: in this case the Nyquist frequency should be 10kHz.
This signal is conditioned by an analog front end stage with an antialiasing filter.
If I implement hardware averaging with 16x oversample, am I actually sampling the signal at 20kHz x16 = 320kHz?
So, if I need at least 60dB of alias attenuation at Nyquist frequency, can I realize the low pass anti aliasing filter so that I have -60dB at 160kHz? Or do I need to have -60dB at 10kHz?
Also, after oversampling, MSPM0G3507 allows to perform averaging: I'm not sure if I understand how decimation is actually a pass-bass filter in this context, and what will be the cutoff frequency of such filter.
Thanks in advance for your replies,
Stefano