This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: How to properly clear ECC errors after sdl_ecc_r5_atcm0 example?

Part Number: AM2634

Tool/software:

I am trying to get a PWM-based-interrupt and a background task to run together with your sdl_ecc_r5_atcm0 example. My current theory is the sdl_ecc_r5_atcm0 example leaves the processor in a constant ECC-error condition, because the fiqExptnHandler is called every ~400ns, which is starving-out my application ISR and background task. 

There are 2 bit-errors caused in the this example, and I if-def-ed out the second single-bit error in ECC_sdlFuncTest. After the double-bit error test has passed, I tried the following calls:

SDL_ecc_aggrWriteEccRamCtrlReg(eccAggrRegs, ramId, 0U);
SDL_ecc_aggrWriteEccRamErrCtrlReg(eccAggrRegs, ramId, 0U, 0U);
SDL_ecc_aggrWriteEccRamErrCtrlReg(eccAggrRegs, ramId, 1U, 0U);
HW_WR_REG32(0x53010020, 0xFF80); //ECC_AGG_TOP_ERR_STAT1

Note eccAggrRegs and ramId were both set in the example code above these calls. 

With the intent of clearing the CTRL, CTRL1, CTRL2, and STAT1 registers in the ECC_AGGR register section. These did not clear any of these registers (all were 1D0 and the CTRL was D0).

What is the proper way to clear the invoked ECC error?

Thanks,

Jim

  • Hello Jim,

    For clearing TCM errors, please do following:

    ATCM: 
    Double bit: Write 0x01 to 0x50D18094 and 0x50D18098
    Single bit:  Write 0x01 to 0x50D18088 and 0x50D18084

    BTCM: 
    Double bit: Write 0x06 to 0x50D18094 and 0x50D18098
    Single bit:  Write 0x06 to 0x50D18088 and 0x50D18084

    These are done in 
    SDL_ESM_applicationCallbackFunction( ) in the file ecc_main.c in the TI provided examples.

    Thanks and Regards,
    Vishwanath Reddy.

  • I did exactly that (that source is in the example), and I expanded the write 0x01 and 0x06 to 0x1F and 0x7F (clearing all bits in those registers). The MCAN ECC example can generate and clear single and double bit errors repeatedly (although I get the occasional data-abort), but these TCM and MSSL2 example will only work on the first single or double bit error, and then the SDL_ESM_applicationCallbackFunction is never called again. This suggests I need to undo the force-error and re-force it, or the interrupt condition is never fully cleared. I am still working this issue, so any suggestions you have would be appreciated. 

    Thanks,

    Jim

  • Hi Jim,

    For TCM memories, once any single bit error is detected, the subsequent errors at the same location will not be detected. This is due to limitation in ARM's RTL  logic.  Once any error is detected, it's corrected value is cached and subsequent access are from it's cache. If you want to repeatedly inject errors in TCM memory, please try below recommendation from ARM:

    - inject error to address A
    - inject error to a different address (not A)
    - inject error to A

     I will check on why MSS_L2 errors are detected second time.

    Thanks and Regards,
    Vishwanath Reddy.

  • Hi Jim, 

    On MSS_L2, I too observed the same behavior. I did some changes to call SDL_ECC_initMemory( ) before the single bit error injection and now I do not see the issue anymore. I can repeatedly inject SEC/DED and able to get ESM interrupts.

    Please find the changes in attached file.

    /*
     *   Copyright (c) Texas Instruments Incorporated 2022-2023
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     */
    
     /**
     *  \file     ecc_trigger.c
     *
     *  \brief    This file contains functions that provide input event triggers
     *            for the Error Correcting Code (ECC) Module application.
     *
     *  \details  ECC Safety Example module tests
     **/
    
    /* ========================================================================== */
    /*                             Include Files                                  */
    /* ========================================================================== */
    #include <stdint.h>
    #include <stdio.h>
    #include <sdl/include/sdl_types.h>
    #include <sdl/sdl_ecc.h>
    #include <kernel/dpl/DebugP.h>
    #include "ecc_main.h"
    #include <sdl/dpl/sdl_dpl.h>
    
    #if defined(SOC_AM263X)
    #include <sdl/include/am263x/sdlr_soc_ecc_aggr.h>
    #endif
    #if defined(SOC_AM263PX)
    #include <sdl/include/am263px/sdlr_soc_ecc_aggr.h>
    #endif
    #if defined(SOC_AM261X)
    #include <sdl/include/am261x/sdlr_soc_ecc_aggr.h>
    #endif
    #if defined(SOC_AM273X)
    #include <sdl/include/am273x/sdlr_soc_ecc_aggr.h>
    #endif
    #if defined(SOC_AWR294X)
    #include <sdl/include/awr294x/sdlr_soc_ecc_aggr.h>
    #include <sdl/include/awr294x/sdlr_intr_esm_mss.h>
    #endif
    
    /* ========================================================================== */
    /*                                Macros                                      */
    /* ========================================================================== */
    /* delay for 1us*/
    #define DELAY 1
    
    /* This macro shows how many ESM events are configured*/
    #define SDL_ESM_MAX_MSS_EXAMPLE_AGGR                (2u)
    #define SDL_MSS_L2_MAX_MEM_SECTIONS                 (1u)
    #if defined(SOC_AM273X) || defined(SOC_AWR294X)
    
    #define SDL_INTR_GROUP_NUM_1                        (1U)
    #define SDL_INTR_GROUP_NUM_2                        (2U)
    #define SDL_INTR_GROUP_NUM_3                        (3U)
    #define SDL_INTR_PRIORITY_LVL_LOW                   (0U)
    #define SDL_INTR_PRIORITY_LVL_HIGH                  (1U)
    #define SDL_ENABLE_ERR_PIN                          (1U)
    
    #define SDL_EXAMPLE_ECC_RAM_ADDR                    (0x10280000u) /* MSS_L2 RAMB address */
    #define SDL_EXAMPLE_ECC_AGGR                        SDL_MSS_ECC_AGG_MSS
    #define SDL_EXAMPLE_ECC_RAM_ID                      SDL_MSS_ECC_AGG_MSS_MSS_L2RAMB_ECC_RAM_ID
    
    #define SDL_MSS_L2_MEM_INIT_ADDR                    (0x02120034u)
    #define SDL_MSS_L2_MEM_INIT_DONE_ADDR               (0x02120038u)
    #define SDL_ECC_AGGR_ERROR_STATUS1_ADDR             (0x02F7c020u)
    #define SDL_ECC_MSS_L2_BANK_MEM_INIT                (0x2u) /* Bank 2*/
    #endif
    
    #if defined(SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
    #define SDL_EXAMPLE_ECC_RAM_ADDR                    (0x70100008u) /*MSS_L2_SLV2 address*/
    #define SDL_EXAMPLE_ECC_AGGR                        SDL_SOC_ECC_AGGR
    #define SDL_EXAMPLE_ECC_RAM_ID                      SDL_SOC_ECC_AGGR_MSS_L2_SLV2_ECC_RAM_ID
    
    #define SDL_MSS_L2_MEM_INIT_ADDR                    (0x50D00240u)
    #define SDL_MSS_L2_MEM_INIT_DONE_ADDR               (0x50D00244u)
    #define SDL_ECC_AGGR_ERROR_STATUS1_ADDR             (0x53000020u)
    #define SDL_ECC_MSS_L2_BANK_MEM_INIT                (0xcu) /*Bank 3*/
    #endif
    /* ========================================================================== */
    /*                            Global Variables                                */
    /* ========================================================================== */
    static SDL_ECC_MemSubType ECC_Test_MSS_L2_subMemTypeList[SDL_MSS_L2_MAX_MEM_SECTIONS] =
    {
         SDL_EXAMPLE_ECC_RAM_ID,
    };
    
    static SDL_ECC_InitConfig_t ECC_Test_MSS_L2_ECCInitConfig =
    {
        .numRams = SDL_MSS_L2_MAX_MEM_SECTIONS,
        /**< Number of Rams ECC is enabled  */
        .pMemSubTypeList = &(ECC_Test_MSS_L2_subMemTypeList[0]),
        /**< Sub type list  */
    };
    
    #if defined(SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
    
    static uint32_t arg;
    
    SDL_ESM_config ECC_Test_esmInitConfig_MAIN =
    {
        .esmErrorConfig = {1u, 8u}, /* Self test error config */
        .enableBitmap = {0x00180000u, 0x00000000u, 0x00000000u, 0x00000000u,
                        0x00000000u, 0x00000000u, 0x00000000u, 0x00000000u},
        /**< All events enable: except clkstop events for unused clocks
         *   and PCIE events */
        /* CCM_1_SELFTEST_ERR and _R5FSS0COMPARE_ERR_PULSE_0 */
        .priorityBitmap = {0x00180000u, 0x000000000u, 0x00000000u, 0x00000000u,
                        0x00000000u, 0x00000000u, 0x00000000u, 0x00000000u },
        /**< All events high priority: except clkstop events for unused clocks
         *   and PCIE events */
        .errorpinBitmap = {0x00180000u, 0x00000000u, 0x00000000u, 0x00000000u,
                        0x00000000u, 0x00000000u, 0x00000000u, 0x00000000u},
        /**< All events high priority: except clkstop for unused clocks
         *   and PCIE events */
    };
    
    extern int32_t SDL_ESM_applicationCallbackFunction(SDL_ESM_Inst esmInstType,
                                                       SDL_ESM_IntType esmIntType,
                                                       uint32_t grpChannel,
                                                       uint32_t index,
                                                       uint32_t intSrc,
                                                       void *arg);
    
    #endif
    
    #if defined(SOC_AM273X) || defined(SOC_AWR294X)
    extern int32_t SDL_ESM_applicationCallbackFunction(SDL_ESM_Inst esmInstType,
                                                        int32_t grpChannel,
                                                        int32_t intSrc,
                                                        void *arg);
    
    /* Event BitMap for ECC ESM callback for MSS L2*/
    SDL_ESM_NotifyParams ECC_TestparamsMSS[SDL_ESM_MAX_MSS_EXAMPLE_AGGR] =
    {
        {
            /* Event BitMap for ECC ESM callback for MSS Single bit*/
            .groupNumber = SDL_INTR_GROUP_NUM_1,
            .errorNumber = SDL_ESMG1_ECCAGGMSS_SERR,
            .setIntrPriorityLvl = SDL_INTR_PRIORITY_LVL_LOW,
            .enableInfluenceOnErrPin = SDL_ENABLE_ERR_PIN,
            .callBackFunction = &SDL_ESM_applicationCallbackFunction,
        },
        {
            /* Event BitMap for ECC ESM callback for MSS Double bit*/
            .groupNumber = SDL_INTR_GROUP_NUM_1,
            .errorNumber = SDL_ESMG1_ECCAGGMSS_UERR,
            .setIntrPriorityLvl = SDL_INTR_PRIORITY_LVL_HIGH,
            .enableInfluenceOnErrPin = SDL_ENABLE_ERR_PIN,
            .callBackFunction = &SDL_ESM_applicationCallbackFunction,
        },
    };
    #endif
    /* ========================================================================== */
    /*                 Internal Function Declarations                             */
    /* ========================================================================== */
    
    /* ECC_Example_init function */
    int32_t ECC_Example_init (void);
    
    /* ========================================================================== */
    /*                          Function Definitions                              */
    /* ========================================================================== */
    
    /*********************************************************************
    * @fn      ECC_Example_init
    *
    * @param   None
    *
    * @return  0 : Success; < 0 for failures
    **********************************************************************/
    int32_t ECC_Example_init (void)
    {
        int32_t retValue=0;
    #if defined(SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
        void *ptr = (void *)&arg;
    #endif
        SDL_ErrType_t result;
        if (retValue == 0) {
            /* Initialize ECC Memory */
            result = SDL_ECC_initMemory(SDL_EXAMPLE_ECC_AGGR, SDL_EXAMPLE_ECC_RAM_ID);
            if (result != SDL_PASS) {
                /* print error and quit */
                DebugP_log("\r\nECC_Test_init: Error initializing Memory of MSS L2 ECC: result = %d\r\n", result);
    
                retValue = -1;
            } else {
                DebugP_log("\r\nECC_Test_init: Initialize of MSS L2 ECC Memory is complete \r\n");
            }
        }
    
        if (retValue == 0) {
            /* Initialize ESM module */
    #if defined(SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
            result = SDL_ESM_init(SDL_ESM_INST_MAIN_ESM0, &ECC_Test_esmInitConfig_MAIN, SDL_ESM_applicationCallbackFunction, ptr);
            if (retValue == SDL_PASS)
            {
                DebugP_log("\r\nESM_Test_init: Init MSS ESM complete \r\n");
            }
            else {
                DebugP_log("\r\nECC_Example_init: Error initializing ESM: result = %d\r\n", result);
                retValue = -1;
            }
            esmError = false;
    #endif
        }
    
        if (retValue == 0) {
            /* Initialize ECC */
            result = SDL_ECC_init(SDL_EXAMPLE_ECC_AGGR, &ECC_Test_MSS_L2_ECCInitConfig);
            if (result != SDL_PASS) {
                /* print error and quit */
                DebugP_log("\r\nECC_Test_init: Error initializing MSS L2 ECC: result = %d\r\n", result);
    
                retValue = -1;
            } else {
                DebugP_log("\r\nECC_Test_init: MSS L2 ECC initialization is completed \r\n");
            }
        }
        return retValue;
    }
    
    /*********************************************************************
     * @fn      ECC_Test_run_MSS_L2RAMB_1BitInjectTest
     *
     * @brief   Execute ECC MSS L2 RAMB 1 bit inject test
     *
     * @param   None
     *
     * @return  0 : Success; < 0 for failures
     ********************************************************************/
    int32_t ECC_Test_run_MSS_L2RAMB_1BitInjectTest(void)
    {
        SDL_ErrType_t result;
        int32_t retVal=0;
    
        SDL_ECC_InjectErrorConfig_t injectErrorConfig;
        volatile uint32_t testLocationValue;
    
    	DebugP_log("\r\nMSS L2 RAMB Single bit error inject: starting \r\n");
    
        /* Note the address is relative to start of ram */
        injectErrorConfig.pErrMem = (uint32_t *)(SDL_EXAMPLE_ECC_RAM_ADDR);
    
        /* Run one shot test for MSS L2 RAMB 1 bit error */
        injectErrorConfig.flipBitMask = 0x002;
        result = SDL_ECC_injectError(SDL_EXAMPLE_ECC_AGGR,
                                     SDL_EXAMPLE_ECC_RAM_ID,
                                     SDL_INJECT_ECC_ERROR_FORCING_1BIT_ONCE,
                                     &injectErrorConfig);
    
        if (result != SDL_PASS ) {
            retVal = -1;
        } else {
            /* Access the memory where injection is expected */
            testLocationValue = injectErrorConfig.pErrMem[0];
    
            DebugP_log("\r\nMSS L2 RAMB Single bit error inject at pErrMem = 0x%p and the value of pErrMem is 0x%p :test complete\r\n",
                       injectErrorConfig.pErrMem, testLocationValue);
        }
    
        return retVal;
    }/* End of ECC_Test_run_MSS_L2RAMB_1BitInjectTest() */
    
    /*********************************************************************
     * @fn      ECC_Test_run_MSS_L2RAMB_2BitInjectTest
     *
     * @brief   Execute ECC MSS L2 RAMB 2 bit Inject test
     *
     * @param   None
     *
     * @return  0 : Success; < 0 for failures
     ********************************************************************/
    int32_t ECC_Test_run_MSS_L2RAMB_2BitInjectTest(void)
    {
        SDL_ErrType_t result;
        int32_t retVal=0;
    
        SDL_ECC_InjectErrorConfig_t injectErrorConfig;
        volatile uint32_t testLocationValue;
    
    	DebugP_log("\r\nMSS L2 RAMB Double bit error inject: starting \r\n");
    
        /* Run one shot test for MSS L2 RAMB 2 bit error */
        /* Note the address is relative to start of ram */
        injectErrorConfig.pErrMem = (uint32_t *)(SDL_EXAMPLE_ECC_RAM_ADDR);
    
        injectErrorConfig.flipBitMask = 0x30002;
        result = SDL_ECC_injectError(SDL_EXAMPLE_ECC_AGGR,
                                     SDL_EXAMPLE_ECC_RAM_ID,
                                     SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE,
                                     &injectErrorConfig);
    
        /* Access the memory where injection is expected */
        testLocationValue = injectErrorConfig.pErrMem[0];
    
        if (result != SDL_PASS ) {
           retVal = -1;
        } else {
            DebugP_log("\r\nMSS L2 RAMB Double bit error inject: pErrMem fixed location = 0x%p once test complete: the value of pErrMem is 0x%p\r\n",
                       injectErrorConfig.pErrMem, testLocationValue);
        }
    
        return retVal;
    }/* End of ECC_Test_run_MSS_L2RAMB_2BitInjectTest() */
    
    /*********************************************************************
     * @fn      ECC_sdlFuncTest
     *
     * @brief   Execute ECC sdl function test
     *
     * @param   None
     *
     * @return  0 : Success; < 0 for failures
     **********************************************************************/
    static int32_t ECC_sdlFuncTest(void)
    {
        int32_t result;
        int32_t retVal = 0;
        uint32_t maxTimeOutMilliSeconds = 1000000000;
        uint32_t timeOutCnt = 0;
    
    
        if (retVal == 0)
        {
    #if defined(SOC_AM273X) || defined(SOC_AWR294X)
            /* Initialize MSS MSS L2 RAMB ESM module */
            result = SDL_ESM_init(SDL_ESM_INST_MSS_ESM, &ECC_TestparamsMSS[0],NULL,NULL);
            /*Clear the global variable before ECC error injecting , in case ESM callback occurred due to any other operation*/
            esmError = false;
            if (result != SDL_PASS) {
                /* print error and quit */
                DebugP_log("\r\nESM_Test_init: Error initializing MSS L2 RAMB single bit ESM: result = %d\r\n", result);
    
                retVal = -1;
            } else {
                DebugP_log("\r\nESM_Test_init: Init MSS L2 RAMB single bit ESM complete \r\n");
            }
    #endif
            /*Inject ECC Single bit error*/
            SDL_ECC_initMemory(SDL_EXAMPLE_ECC_AGGR, SDL_EXAMPLE_ECC_RAM_ID);
            result = ECC_Test_run_MSS_L2RAMB_1BitInjectTest();
    
            if (result == SDL_PASS)
            {
                DebugP_log("\r\nWaiting for ESM Interrupt\r\n");
                do
                {
                    timeOutCnt += 1;
                    if (timeOutCnt > maxTimeOutMilliSeconds)
                    {
                        result = SDL_EFAIL;
                        break;
                    }
                } while (esmError == false);
            }
            if(result == SDL_PASS){
                DebugP_log("\r\nUC-1: Injected 1-bit error and got ESM Interrupt \r\n");
                esmError = false;
            }
    
            if (result != SDL_PASS) {
                retVal = -1;
                DebugP_log("\r\nESM_ECC_Example_run: UC-1 has failed...\r\n");
                /* UC-1 Low priority MSS L2 interrupt */
            }
        }
        if (retVal == 0) {
    
    #if defined(SOC_AM273X) || defined(SOC_AWR294X)
            /* Initialize MSS MSS L2 RAMB ESM module */
            result = SDL_ESM_init(SDL_ESM_INST_MSS_ESM, &ECC_TestparamsMSS[1],NULL,NULL);
            /*Clear the global variable before ECC error injecting , in case ESM callback occurred due to any other operation*/
            esmError = false;
            if (result != SDL_PASS) {
                /* print error and quit */
                DebugP_log("\r\nESM_Test_init: Error initializing MSS L2 RAMB single bit ESM: result = %d\r\n", result);
    
                retVal = -1;
            } else {
                DebugP_log("\r\nESM_Test_init: Init MSS L2 RAMB single bit ESM complete \r\n");
            }
    #endif
    
    #if defined(SOC_AM273X) || defined(SOC_AWR294X) || defined (SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
            /* Initialize ECC Memory */
            SDL_ECC_initMemory(SDL_EXAMPLE_ECC_AGGR, SDL_EXAMPLE_ECC_RAM_ID);
    #endif
            /*Clear the global variable before ECC error injecting , in case ESM callback occurred due to any other operation*/
            esmError = false;
    
            /*Inject ECC Double bit error*/
            result = ECC_Test_run_MSS_L2RAMB_2BitInjectTest();
    
            if (result == SDL_PASS)
            {
                DebugP_log("\r\nWaiting for ESM Interrupt \r\n");
                do
                {
                    timeOutCnt += 10;
                    if (timeOutCnt > maxTimeOutMilliSeconds)
                    {
                        result = SDL_EFAIL;
                        break;
                    }
                } while (esmError == false);
            }
            if(result == SDL_PASS){
                DebugP_log("\r\nUC-2: Injected 2-bit error and got ESM Interrupt\r\n");
                esmError = false;
            }
    
            if (result != SDL_PASS) {
                retVal = -1;
                DebugP_log("\r\nESM_ECC_Example_run: UC-2 has failed....\r\n");
                /* UC-2 High priority MSS L2 interrupt */
            }
        }
    
        return retVal;
    }
    
    /*********************************************************************
     * @fn      sdlApp_dplInit
     *
     * @brief   Initialization of DPL
     *
     * @param   None
     *
     * @return  0 : Success; < 0 for failures
     **********************************************************************/
    static int32_t sdlApp_dplInit(void)
    {
        SDL_ErrType_t ret = SDL_PASS;
    
        ret = SDL_TEST_dplInit();
        if (ret != SDL_PASS)
        {
            DebugP_log("\r\nError: Init Failed\r\n");
        }
    
        return ret;
    }
    
    /* ECC Function module test */
    int32_t ECC_funcTest(void)
    {
        int32_t testResult = 0;
    
        /*Initializing the DPL*/
        sdlApp_dplInit();
    
    #if defined(SOC_AM263X) || defined(SOC_AM263PX) || defined (SOC_AM261X)
        /* Clear Done memory*/
        SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_DONE_ADDR, 0xfu);
    #endif
    
        /* Initialization of MSS L2 memory*/
        SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_ADDR, SDL_ECC_MSS_L2_BANK_MEM_INIT);
    
        while(SDL_REG32_RD(SDL_MSS_L2_MEM_INIT_DONE_ADDR)!=SDL_ECC_MSS_L2_BANK_MEM_INIT);
    
        /* Clear Done memory after MEM init*/
        SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_DONE_ADDR, SDL_ECC_MSS_L2_BANK_MEM_INIT);
    
        /*Clearing any old interrupt presented*/
        SDL_REG32_WR(SDL_ECC_AGGR_ERROR_STATUS1_ADDR, 0xF0Fu);
    
    
        /*Initializing required modules*/
        testResult = ECC_Example_init();
    
        if (testResult != SDL_PASS)
        {
            DebugP_log("\r\nECC Safety Example tests: unsuccessful\r\n");
            return SDL_EFAIL;
        }
    
        /*Execute ECC sdl function test*/
        while(1)
        {
            testResult = ECC_sdlFuncTest();
        }
    
        return (testResult);
    }
    
    /* Nothing past this point */
    

    I'm checking internally on the observed behavior. Will share info as soon as I get more details.

    Thanks and Regards,
    Vishwanath Reddy.