Part Number: AM2431
Tool/software:
Please provide the accuracy of the MCU_RC_OSC_12M frequency.
This information is needed when using a Dual Clock Comparator.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2431
Tool/software:
Please provide the accuracy of the MCU_RC_OSC_12M frequency.
This information is needed when using a Dual Clock Comparator.
II suspect the document that says the limit is ±10% was simply rounded to the nearest whole number.
The nominal frequency is 12.55MHz. The upper limit provided in my previous reply represents a variation of [(13.81MHz/12.55Mz) - 1] x 100 = 10.04%. The lower limit provided in my previous reply represents a variation of [(11.25MHz/12.55Mz) - 1] x 100 = -10.36%. The limits I provided are very close to ±10%.
Regards,
Paul