Part Number: TM4C1230E6PM
Tool/software:
Hi,
Im trying to make a timer which periodically triggers an interrupt on a TM4C1230E6PM.
Here is the minimal example I came up with:
// --- Includes
#include <stdio.h>
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "driverlib/timer.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
// --- Typedefs
typedef void (*pFctHandler)(void);
typedef const struct
{
uint8_t TIMER_NR;
uint32_t SYSCTL_TIMER;
uint32_t TIMER_BASE;
uint32_t TIMER_CFG;
uint32_t TIMER_A_OR_B;
uint32_t TIMER_INTERVAL_US;
uint32_t INT_FLAGS;
pFctHandler callbackFct;
} timerHW_t;
// --- Local Function Prototypes
void test_tick(void);
// --- Variables
timerHW_t tmr =
{
.TIMER_NR = 0,
.SYSCTL_TIMER = SYSCTL_PERIPH_TIMER2,
.TIMER_BASE = TIMER2_BASE,
.TIMER_CFG = TIMER_CFG_PERIODIC,
.TIMER_A_OR_B = TIMER_BOTH,
.TIMER_INTERVAL_US = 1000, // not implemented
.callbackFct = test_tick,
.INT_FLAGS = TIMER_TIMA_TIMEOUT,
};
int main(void)
{
// Set Clock
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //80MHz SysClk
// Enable Interrupts
IntMasterEnable();
// Enable the peripheral
SysCtlPeripheralEnable(tmr.SYSCTL_TIMER);
// Wait for the module to be ready.
while(!SysCtlPeripheralReady(tmr.SYSCTL_TIMER))
{
}
// configure Timer
TimerConfigure(tmr.TIMER_BASE, tmr.TIMER_CFG);
TimerLoadSet(tmr.TIMER_BASE, tmr.TIMER_A_OR_B, SysCtlClockGet());
// Register the interrupt handler
TimerIntRegister(tmr.TIMER_BASE, tmr.TIMER_A_OR_B, tmr.callbackFct);
// Start the timer
TimerEnable(tmr.TIMER_BASE, tmr.TIMER_A_OR_B);
TimerIntEnable(tmr.TIMER_BASE, tmr.INT_FLAGS);
while(1)
{
// do nothing
;
}
}
void test_tick(void)
{
TimerIntClear(tmr.TIMER_BASE, tmr.INT_FLAGS);
// Why is this line needed?
TimerLoadSet(tmr.TIMER_BASE, tmr.TIMER_A_OR_B, SysCtlClockGet());
}
I have the following problems with this:
- Why is the line 81 needed? Should the Timer with TIMER_CFG_PERIODIC not reset itself when load 0 is reached? Without this line I'm basically stuck in test_tick()
- With Line 81 active, I noticed that the Clock Counts between line 78 is inconsistent. Its often around the expected 80 000 000 (80 000 192) but deviates in between it shows [0 (???), 70 000 000, 68 000 000, 79 000 000]. Shouldn't the timer be very exact in how many Clock cycles happen between calls?
Thanks for any help in advance!