Tool/software:
Dear TI experts,
I know that the PA0 and PA1 have both a 5V open drain, is it possible to combine the PWM capabilities with a 5V max output? Although I have changed the jumpers appropriately for this function(I have tried out all configs), I don't seem to reach the 5V.
Furthermore, if a PWM with 5V max output is not possible on PA0/PA1, are there other pins, also in the debugging board, which could serve this purpose? I require a 5V PWM output for an application.
Kind regards,
Vanessa