Part Number: LP-MSPM0L2228
Tool/software:
Dear expert,
SDK version: mspm0_sdk_2_01_00_03
Example running from SDK without any modify: lcd_write_memory
User run with the LCD example from our SDK, and powered with XDS110 through USB cable.
Sometimes the LED4 will light up with light blue and the LCD won't work well,
and we have to trigger the reset buttom then it will work well.
If you can't duplicate this, you can remove the power and do this again until it is triggered.
I am thinking this may refer to the power sequence of LCD?
Best Regards,
Eric Chen