This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: SPI Implementation guides.

Part Number: TMS570LS1224

Tool/software:

Hi 

I am using the ,Hercules Launch Pad Development Kit

When I generated code using the HAL Co Gen and I enable 2 SPI ( SPI1 and SPI4). 

Easy to locate SPI4 pins in the J11 connector, so I configured it. 

When I run the code after all the connection made, the code struck at the place where "while((spi->FLG & 0x00000100U) != 0x00000100U)"

Pls help me if there any configuration to be noted while configuring , and I prefre the pooling mode instead of the interrupt mode as the begining. 

pls suggest. 

Thanks.

  • Hi Ramesh,

    We have some working SPI and mibspi examples in below FAQ:

    Please refer them once and make sure the configurations. If it doesn't solve the issue, then i will do further investigation and if necessary, we can set one live debugging session as well.

    --
    Thanks & regards,
    Jagadish.