Part Number: MSPM0C1104
Other Parts Discussed in Thread: MSP430G2452
Tool/software:
Hello,
I'm using pwm output on a MSPm0C1104 launchpad.
I use the pwm dead band example:tima_timer_mode_pwm_dead_band_LP_MSPM0C1104_nortos_gcc.
All pins are unloaded.
But my signal don't go up to 3.3V (Vdd-0.5V) and down to 0 Volts (Vss+0.4V). So the signal has only a 2.4V swing. It is in the limits of the specs.
Is it normal without a load (I=0mA)?
Best regards. Nicolas.
Here are 1 screenshots, one at 60kHz and one at 2kHz.
c