Part Number: AM2634
Tool/software:
Hi Team,
Query form the customer on using NAND flash with AM2634. The device planned is HY27UF084G2B-TPCB (Hynix, 512MB , x 8 bit, 25 ns).
With respect to the read or write cycles shown in AM2634 datasheet ( Fig 7-36 to Fig 7-39), the devices are compatible.
But no Ready/busy pin is given on the processor for GPMC.
So, can the Ready/busy pin of the NAND flash be connected to any GPIO or you suggest a specific pin?
And can we use any chip select, ie say GPMC Chip Select 0 (GPMC0_CSn0) for NAND flash?
Regards,
Chander